Post Go back to editing

AD9914的同步

Thread Summary

用户在使用CPLD配置两片AD9914芯片输出300多兆的正弦连续波时遇到相位差不一致的问题,尽管时钟输入和配置相同。最终建议用户联系ADI技术支持邮箱获取进一步帮助。用户尝试了两种配置时钟的选择(100M和133.33M)但均未解决问题,且发现AD9914手册中未提及同步相关内容。
AI Generated Content

我现在使用CPLD配置贵公司的两片ad9914芯片实现输出300多兆的正弦连续波,现在基本波形已经输出,两片的配置完全一样,但是每次上电或者复位之后,两片的相位差均不一样。  

    具体情况为:两片AD9914采样3.2G的直接时钟,不用内部的锁相环,两片时钟输入完全一样。采用并口配置,profile模式,相位偏移两片都设置为0。

    我按照ADI网站上的应用笔记《AN-1254:同步多个基于DDS的频率合成器AD9915》参见上图中的步骤 进行的同步配置,但是由于AD9914没有AD9915的同步DAC CAL 和编程SYNC_OUT的延迟位,所以5、6的步骤没有做,其他步骤都有完成。硬件电路上,芯片1作为主芯片输出SYNC_OUT,经过同样长度的路径输入给芯片1和芯片2的SYNC_IN。用探针采到的sync_in引脚在示波器的输出是同步的,但是每次上电或者复位之后,两片的相位差均不一样。

    请问AD9914的同步和AD9915有什么不同,还需要进行怎样的配置,或者检查哪些信号。

    另,我还有几个问题不太清楚:

    1. 应用笔记上说:各器件的IO_UPDATE必须与SYNC_CLK同步,是说IO_update的上升沿和SYNC_CLK的上升沿要对齐吗,我有尝试用SYNC_CLK锁存器锁一级

    2.我现在配置AD9914的时钟有两种选择,一个是外部输入的与3.2G的参考同源的100M时钟,还有一个是9914输出的sync_clk 133.33M的时钟,请问选择哪个比较好,我现在两个都尝试过,都不能实现同步的要求。

    附件为从ADI网站下载的应用笔记AN-1254,请参考。

AN-1254_cn.pdf

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.