Post Go back to editing

AD9837主时钟问题

Thread Summary

用户询问AD9837是否可以在不使用外部MCLK的情况下工作。ADI工程师确认AD9837必须外加时钟到MCLK,寄存器D7的设置仅控制外部MCLK是否导通进入芯片内部。
AI Generated Content

最近开始接触使用DDS芯片AD9837,仔细阅读了手册,然后画板子,写程序,最终出来还是遇到了问题。

控制寄存器中D7=0时,使能内部MCLK,按照我的理解,就是指AD9837可以不用外部输入MCLK,但是实际情况并非如此,无论怎么配置寄存器,只要没有外部MCLK输入,DDS就不会输出,于是飞线输入外部MCLK,工作正常了。

我需要专家来明确一个事情:AD9837是不是必须要外部MCLK才能工作?如果不是,应该怎么配置?

谢谢~

Parents Reply Children
No Data