Post Go back to editing

AD9524 PLL1无法锁定,PLL1 OUT无信号

Thread Summary

The user encountered no output from PLL1_OUT on the AD9524 when using a 25 MHz VCXO, despite observing a 25 MHz clock at OSC_IN. The final answer suggests checking the PLL1 loop parameters and ensuring REG0x1BA and REG0x1BB are not powered down. The accompanying answer recommends verifying the PLL1 lock status and providing the .stp configuration file and VCXO data sheet for further assistance.
AI Generated Content

问题1:如图中红框部分。VCXO使用25M晶振。设置D1后,PLL1_OUT没有输出?这个PLL1_OUT不需要再做其它处理吧?用示波器量9524的OSC_IN有25M时钟,但PLL1_OUT没有输出?

   

问题2:回读ox22c=0xe6,显示PLL1未锁定,各位原来9524的PLL1没锁定的,最后都是怎样锁定的?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.