AD9523-1无法输出时钟

在使用AD-FMCDAQ2-EBZ开发板上的AD9523-1芯片时遇到问题。AD9523-1芯片工作于PLL2单环路状态下,输入晶振125MHz,关键寄存器设置如下:R2=1,X2=0,A=0,B=6,M1=M2=3,设置完毕进行VCO校正后查看状态寄存器,PLL2 LOCKED=1,VCXO状态OK,PLL2 Reference clk状态OK,就是PLL2 feedback clock状态为0,也就是说回读寄存器0x22C的值为0xA2,0~3路直接接到VCXO,可以正常输出,把0~14路输出全部接M1分频器,全部没有输出,4~9路接入M2分频器,也没输出。问题出在哪里,哪位大神帮忙指导一下。那个PLL2 feedback clock是指的那个时钟?为何该时钟没有,而PLL2可以正常LOCKED?

Parents Reply Children
No Data