关于两片AD9739的同步问题

我们在做一个调制器相关项目,用了两片AD9739,分别做I/Q两路输入到调制芯片ADL5386,有两个问题麻烦解答:

  1. 两片AD9739SYNC INOUT实现同步,AD9739-1的OUT作为BUFER的输入,BUFER的输出分别接两片9739的IN,AD9739-2的OUT悬空,这样连接是否正确?这些同步信号是否还需要接到FPGA中去被控制?实现同步的BUFFER1.8V ADCLK846是否可以?
  2. AD9739位70欧姆输出阻抗,而ADL5386位50欧姆输入阻抗,两者之间连接请问如何做阻抗匹配?还要保证ADL5386为500MV直流偏置?
  3. 在论坛上看到有同行说调试时出现9739的一些问题是由于DACCLK没有用手册中推荐的ADCLK914,我们现在设计的是ADF4351输出差分时钟经过ADCLK925给俩片ADA9739,请问这样接是否可以?