Post Go back to editing

about AD9540

Thread Summary

用户询问是否可以使用AD5460生成1~100MHz的时钟,频率分辨率为1Hz。AD9540最高输出频率为655MHz,分辨率2.33uHz,集成DDS和PLL,DDS最高工作速度为400MHz,可直接合成高达160MHz的信号。AD9540的两个滤波器分别用于PLL的稳定控制电压生成和DDS输出的抗混叠滤波,建议参考AD9540评估板原理图和使用ADISimCLK仿真计算环路滤波器,用ADS设计抗混叠滤波器。
AI Generated Content

我想使用贵公司的AD5460产生一个时钟,我想的得到的频率范围是1~100MHz,频率分辨率为1Hz,可以吗?