Post Go back to editing

AD9910 DRG模式调试

Thread Summary

用户在使用单片机调试AD9910时,尝试实现1M到21M的10ms扫频,但示波器显示的输出仅为186kHz的100多毫伏正弦波。最终答案建议查阅DDS常见问题解答,以解决配置问题。用户还询问了振幅设置的寄存器位置和循环扫频的配置方法。
AI Generated Content

使用单片机调试AD9910,想实现1M到21M的扫频,扫频总时间为10ms,相关的寄存器配置如下,最后用示波器看只输出了一个峰峰值在100多毫伏的正弦波,频率是186khz,不解,希望各位工程师看看,寄存器哪里配置有问题,

const uchar cfr1[]={0x00,0x40,0x00,0x00};       //cfr1控制字

const uchar cfr2[]={0x01,0x4c,0x08,0x20};       //cfr2控制字

const uchar cfr3[]={0x04,0x0F,0x41,0x28};       //cfr3控制字  40M晶振  20倍频  VC0=100   ICP=001;

uchar DRL[]={0x01,0x40,0x6f,0x40,0x00,0x0f,0x42,0x40}; //数字斜坡限值1MHZ~21MHZ

uchar DRS[]={0x00,0x00,0x00,0xc4,0x00,0x00,0x00,0xc4}; //数字斜坡步进值100HZ

uchar DRR[]={0x00,0x0a,0x00,0x0a}; //斜坡速率10ms,即单次频率持50ns

另外有两个问题:

1.扫频源的振幅设置是在哪个寄存器?

2.如果我想循环扫频,即从1M扫到21M,在跳回1M,重新扫,有没有相关的寄存器配置呢(在不使用中断,循环的前提下)?