[ADI microblogging question and answer selection] A series of 0 ohm resistors on the RF trace will not affect the RF signal by ADIForum
@IRON 愚人J : Hello, there is a question I would like to ask. Recently , I was designing the PLL circuit. I saw that there is a 0 ohm resistor on the final RF output branch of the reference design of the ADF4350 . Please connect it in series on the RF trace. Does a 0 ohm resistor not affect the RF signal?
ADI Expert : Hello! When the frequency is high, it will affect the result. Therefore, it is usually recommended to leave enough debug pads in the first version, which can be debugged, such as matching networks. After the experiment, determine the final network and topology results, at which point the design PCB should remove unnecessary debug pads.