Post Go back to editing

MAX78000

Thread Summary

用户询问MAX78000中CNN数据输入地址的确定方法以及digit-detection-demo示例使用的模型。最终答案指出地址是通过C代码生成器自动生成的,可以在生成的cnn_unload()函数中查看。digit-detection-demo使用的模型可能是ai85net-tinierssd.py,遇到YAML错误时应参考官方文档。
AI Generated Content

1:MAX78000中此类地址是如何确定的?

   您好,我明白这是CNN数据输入的地址,但是我不太明白这个地址是怎么产生的,而且每一个Dome中的这个地址不尽相同,请问是通过ai9xize.py自动生成的地址?我应该如何去选择这个地址?

2:Examples/MAX78000/CNN/digit-detection-demo这个dome是如何生成的使用的是哪一个模型?我注意到是ssd的所以我尝试使用官方训练过的生成c代码的时候出现了问题,由于我没有充分关于神经网络的知识,请问这个错误要怎么解决,digit-detection-demo所以的模型是哪一个?

Parents
  • 因为您截的图是一部分,您这个第一个图里面的代码是哪个代码或者工程里面的,请发一下链接。关于第二个SSD的模型,我个人认为是https://github.com/MaximIntegratedAI/ai8x-training/blob/develop/models/ai85net-tinierssd.py (但我还需再确认一下。)

  • 您好,1中图片为\MaximSDK\Examples\MAX78000\CNN\mnist中的void load_input(void)函数,我只是根据需要修改了一部分,但是这个0x50400000这个地址是没有修改的,所以疑惑这种地址是怎么产生的,2中如果模型为ai85net-tinierssd.py的话那么使用ai8xize.py中所需要的networks所对应的,yaml文件是哪一个?

Reply
  • 您好,1中图片为\MaximSDK\Examples\MAX78000\CNN\mnist中的void load_input(void)函数,我只是根据需要修改了一部分,但是这个0x50400000这个地址是没有修改的,所以疑惑这种地址是怎么产生的,2中如果模型为ai85net-tinierssd.py的话那么使用ai8xize.py中所需要的networks所对应的,yaml文件是哪一个?

Children