Post Go back to editing

MAX78000

Thread Summary

用户询问MAX78000中CNN数据输入地址的确定方法以及digit-detection-demo示例使用的模型。最终答案指出地址是通过C代码生成器自动生成的,可以在生成的cnn_unload()函数中查看。digit-detection-demo使用的模型可能是ai85net-tinierssd.py,遇到YAML错误时应参考官方文档。
AI Generated Content

1:MAX78000中此类地址是如何确定的?

   您好,我明白这是CNN数据输入的地址,但是我不太明白这个地址是怎么产生的,而且每一个Dome中的这个地址不尽相同,请问是通过ai9xize.py自动生成的地址?我应该如何去选择这个地址?

2:Examples/MAX78000/CNN/digit-detection-demo这个dome是如何生成的使用的是哪一个模型?我注意到是ssd的所以我尝试使用官方训练过的生成c代码的时候出现了问题,由于我没有充分关于神经网络的知识,请问这个错误要怎么解决,digit-detection-demo所以的模型是哪一个?