电路中ADN8831接TEC正极的那两个MOS管为集成的FDW2520,上电之后有控温,栅极处有PWM波占空比的变化,但是MOS管发热异常,之前不会很烫,会是什么问题?电路如附件图片中,其中MOS管型号为FDW2520
9脚和18脚,我采用了典型电路的方法,中间使用了5欧姆的电阻。这里有两个问题。1、您的TEC两端的电压是3.3V,而根据您的电路图,加热电流限制(ILIMH,Pin32)为1.15A,一般TEC的工作时需要12V电压,2A的电流,您的TEC能工作起来吗?2、请问您的电路现在调出来了吗?可不可以帮我看一下,遇到瓶颈了。下面是主要引脚的电压状态(图传不上去,只能用文字的方式),LPGATE(Pin 25…
看看OUT2的电压是多少,进一步可以看看IN2P和IN2N的电压各是多少。
看起来像是温度反馈无法跟上温度的给定。环路稳定之后IN2P和IN2N是一致的。