ADL5380基带输出为50 ohm差分阻抗,但为什么参考电路用的是9:1的巴伦,问过支持,怎么说是什么负载是450 ohm,然后用9:1转,但是手册上的差分输出50 ohm又是什么意思,如果是50ohm,我想用个1:1的转成单端50ohm可以么。 另IQ调制时,用单端转巴伦,1:1的怎么接共模电压
ADL5380基带输出为50 ohm差分阻抗,但为什么参考电路用的是9:1的巴伦,问过支持,怎么说是什么负载是450 ohm,然后用9:1转,但是手册上的差分输出50 ohm又是什么意思,如果是50ohm,我想用个1:1的转成单端50ohm可以么。 另IQ调制时,用单端转巴伦,1:1的怎么接共模电压
ADL5380的中频输出阻抗是50ohm,可以接1:1的balun,EVB使用的是9:1balun,意味着ADL5380所带的是450ohm的负载(50*9=450 ohm),非DC 耦合,不用考虑共模电压
EVB使用的是9:1balun,要出450ohm,应该是balun主级接基带50ohm,次级接负载吧?这样才是(50*9=450 ohm)吧,按EVB接,应该是50/9吧
balun输出一般接50ohm阻抗的频谱仪,这样在ADL5380的load是450ohm