视频介绍:低输入偏置电流高共模抑制比FET输入的高速仪用放大器CN0273

视频介绍:低输入偏置电流高共模抑制比FET输入的高速仪用放大器CN0273 by adiadmin

该电路是一款高速FET输入、增益为5的仪表放大器,具有35 MHz宽带宽和10 MHz时55 dB的出色交流共模抑制(CMR)性能。该电路适用于需要高输入阻抗、快速仪表放大器的应用,包括RF、视频、光学信号检测和高速仪器仪表。高CMR和高带宽特性还使其成为宽带差分线路接收器的理想选择。

点击播放视频

 

CN0273电路笔记下载:

http://www.analog.com/static/imported-files/circuit_notes/CN0273.pdf

 

 

CN0273详细介绍:

http://www.analog.com/zh/circuits-from-the-lab/CN0273/vc.html

 

 

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.