MAX16840在REFI内部有一个50uA的电流源,对于MAX16840LEVKIT的电路来说,这个电流源的电流同时流向R6和Q1的3脚,而流向Q1的3脚的电流取决于输入电压和电阻R2的大小,R2的值是固定的,所以当输入电压变化时会引起Q1的3脚电流的变化,流过R6的电流也会改变,从而改变REFI处的电压。例如,当输入从10V增加到12V后,流入Q1的3脚的电流增大,流向R6的电流减小,REFI的电压减小,所以FB=VREFI/6的电压也减小,LED的电流减小,整个电路的输入电流也减小,从而保证输入功率固定。但是这个电路会使LED电流随着输入电压的改变在±10%范围内波动。