ADP7105芯片内部误差放大器的基准源与数据手册上的不同。经过多次测试,结果是基准电压为0.273V和数据手册上的1.22V相差较大,造成在我们系统第一版这块都不能用了,下一个版本中不敢使用。
一年前的方案测试结果和现在的结果一样,原来设计方案是输入12V,通过外部反馈电阻调整输出为11V,但是实测输出是2.4V左右。通过不断更改电阻调整输出到11V时,测试FB管脚电压为0.273V。这个电压应该就是对应的内部误差放大器中基准源的电压。但是这个结果和数据手册上的信息不同。不知道这样能用吗?