Post Go back to editing

LT4363-2: MOSFET turns off during 70V/30µs pulse but TMR pin stays at 0.5V (not charging)

Category: Hardware

Hello ADI EngineerZone,

I am simulating the LT4363-2 in LTspice for an overvoltage protection application. When I apply a 70V/30µs pulse to the input, the MOSFET is turned off (GATE is pulled low, VOUT drops). However, I observe that the TMR pin voltage remains at 0.5V and never charges up.

According to the datasheet, during a fault the TMR capacitor should charge from 0.5V to 1.275V (early warning) and then to 1.375V before the MOSFET is turned off. Since TMR is not charging, why is the MOSFET still turned off?

Could there be another internal mechanism that turns off the MOSFET without activating the TMR timer? Or is this behavior an artifact of the LTspice model?

I have attached the schematic and simulation waveforms (GATE, VOUT, TMR, OV, SNS-OUT). Any insight would be greatly appreciated.

Thank you.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.