Post Go back to editing

请教LTC7878使用电阻采样rsns的方案电流纹波问题

Thread Summary

The user reports current ripple and fluctuation in the average current on the LTC7878 demo board, especially at specific operating points. The final answer suggests reducing the capacitance of C378 to 4.7nF or 2.2nF to mitigate sampling delay, or increasing Vin to 60V to reduce PWM duty cycle near 100%. The issue might also be due to noise modulation on the low-level ISNS differential sampling signal.
AI Generated Content

1、如图中,ch1 Vin 50V, CH4 Vo 43V负载CV, CH3 IL,频率100kHz,恒流5A输出。目前看到的问题是,在一些特定的工作点,出现类似上图的电流的大小波点情况。谷值电流相差0.3A,在平均电流上也观察到明显的波动。从这个带宽来看,并不是环路问题,而像是电流采样的控制部分引起的。

2、BBU-12kW,原理图参考demo板,关键参数如下:电感电流采样,串联了采样电阻10mOhm,RC滤波参数为51Ohm-1nF/10nF; Mode 配置成 100mV CCM,外部RC对GND的参数为10k 1nF,应不会有电平问题;Ith引脚的环路配置,参数如下,暂未实测,但电压环路的带宽是稳定的且带宽较低,按照ith的RC计算,理论上不会导致大小波;

                    

3、这个电流纹波在demo板测试也有,负载CV,Vin 45V, Vout分别为43V和48V,电感电流包络也有点波动;

     

  • 可能是电流采样滤波过重导致的采样延迟,把C378=10nF改成4.7nF,或者2.2nF,看看是否缓解;也有可能是Vin≈Vo时PWM占空比接近100%,把Vin拉到60V,看看大小波是否减轻;也可能ISNS差分采样信号只有几十mV,这个信号很容易受到几mV的噪声调制
  • 感谢回复,1、LTC7878使用电阻采样rsns的方案电流纹波问题,可能是电流采样滤波过重导致的采样延迟,把C378=10nF改成4.7nF,或者2.2nF,看看是否缓解;

    -- 经验证,并未变好,部分电压点变差;

     2、也有可能是Vin≈Vo时PWM占空比接近100%,把Vin拉到60V,看看大小波是否减轻;

    -- 实际应用,Vin不变,Vo变化。附件中Vo调节从41~56V,Vin保持50V。看起来41Vin时Duty是原理100%的,但包络震荡反而比较明显。

     3、也可能ISNS差分采样信号只有几十mV,这个信号很容易受到几mV的噪声调制,

    -- 这个目前cbc/isns电阻均用的比较大了。信号幅值约为50mV,且layout上按照开尔文连接&差分走线。

    -- 另一方面,在某些工作点下,也有包络较为稳定的情况,如果是layout上受扰,应全范围内都有明显震荡。

    请协助从内部原理上协助分析,谢谢!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.