Post Go back to editing

四路级联LT8292时,电流不能平均分配的原因?

测试环境(升压):输入31-43V,输出46.5V,四个芯片单独可以达到20A,但是四个级联时,电流不能平均分配,如下:备注1:虽然电流不能平均,但是所有的波形很固定

  U1 U3 U2 U4
28.2A 8.7A 8.7A 5.4A 5.4A
41.4A 12.7A 12.7A 7.98A 7.98A
55.4A 17.3A 17.3A 10.7A 10.7A