Post Go back to editing

LT8316HFE#PBF高温测试时烧毁MOS管问题

Thread Summary

用户在使用LT8316HFE#PBF设计400V转24V的直流模块时,发现MOSFET Q1在140℃高温下烧毁。建议检查MOSFET的结温,可能已超过150℃的最高允许温度,考虑增加散热片或风扇以改善散热。
AI Generated Content
Category: Hardware
Product Number: LT8316HFE#PBF, LT8316

最近在使用LT8316HFE#PBF做一个直流400V转24V的模块,电路是按照手册推荐的电路设计的,详见下图,反激变压器是定制的,目前常温测试没有问题,当温度升高到140℃时mos管Q1就烧掉(带载约0.92A),不知道什么原因,将这个mos管换成低导通内阻的在高温时也烧,请大神帮忙指导一下,不知哪里出的问题