Post Go back to editing

芯片会影响输入电压的稳定性

Thread Summary

The user experiences increased ripple (18mV) at 900kHz when powering an LT3094 LDO from a -15V input with 7mV ripple. The final solution suggests replacing the 100uF input capacitor with a 10uF low ESR ceramic capacitor to reduce the ripple.
AI Generated Content
Category: Hardware
Product Number: LT3094

我的输入电压是-15V,纹波在7mV,但是我只要给LT3094供电,马上就会产生18mV的纹波,频率在900kHz左右,阶跃信号,并不是很方正。LDO输出-14V,PGFB是接输入电源,ILIM是接地,PG浮空,输入电容是100uf(去掉也没用),输出电容是10uf+0.1uf,再经过一个保险丝

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.