Post Go back to editing

LTM4678电压输出上限问题

问题1:

是否可以往liao36l@qq.com这个邮箱发送一个Run LTpowerPlay license,在软件界面申请了几次都无回复。

问题2:

现象:

我使用FPGA对LTM4678进行配置。配置VOUT_COMMAND寄存器时,只要配置电压大于2.75V,就会出现输出电压不稳定的情况。

过程:

我已经对如下寄存器进行配置:VOUT_OV_FAULT_LIMIT(配置为3.4V),VOUT_MAX(默认为3.6V),MFR_PWM_MODE(配置为0xC5),MFR_PWM_CONFIG(默认为0x10),并对寄存器进行了回读,都是对应数据,如上这几个寄存器我认为和输出电压有直接关系。

结果:

对MFR_VOUT_MAX寄存器回读一直为2.75V,相当于默认值就为2.75V,与手册上的3.6V不一致。并且手册上对寄存器的描述中,此寄存器只与MFR_PWM_CONFIG的bit6有关,在上面的配置过程中,我已经保证MFR_PWM_CONFIG的bit6为0了。我想请问下是否还有什么寄存器会对MFR_VOUT_MAX的值有影响,然后我前面的现象有可能是因为这个寄存器引起的吗。

Parents Reply Children