Post Go back to editing

ADP5071输入电压=+12V、输出电压=±26.5V,输出异常

Category: Hardware
Product Number: ADP5071

问题描述:一款通过ADP5071输出±26.5V(输入电压=+12V)、然后分别通过LT3080和LT3091降压到+25V和-25V的板子,输出电压异常;

刚上电时,ADP5071的正负电压都有输出分别为+25.9V、-27.2V,LT3080和LT3091输出分别为+25.2V和-25.3V;(此时Vreg=4.11V,Vref=1.6V) ←此时各电压正常;

但是ADP5071温度较高大约在48°,之后会慢慢上升,经过2-3分钟之后输出电压降至0V,此时ADP5071温度升高至93°(感觉像是过载导致短路,但将负载端连接的OP-AMP断开也是一样。。。)

其余管脚参数设定如下:

[EN1/EN2] 10kΩ上拉至Vin;

[SYNC/FREG] 0Ω下拉至GND;→1.2MHz

[SLEW] 悬空;→快速启动

[SEQ] 0Ω上拉至VREG;→±同时启动

[COMP1] 补偿网络R=4.7kΩ,C=47nF;

[COMP2] 补偿网络R=15kΩ,C=47nF;

另:按下记电路参数配置,使用LTspice仿真可正常输出±26.5V;

第一次使用ADP5071不明白是什么原因,望各位高人给与指导,谢谢。

Parents Reply Children
  • 您提及2点、耐压范围和COMP2补偿网络,有道理。经过调试(更换电感、调节COMP1和2的RC值),目前ADP5071温度大致在45°左右,虽然发热不严重但感觉还是有些高。。。

    1.针对开关管耐压40V问题,我通过外部DC直流源作为输入,

       ①将Vin调整至11V时,ADP输出分别为+25.8V、-27V,ADP5071温度降至37°,SW1和2波形如下:

      ②将Vin调整至10V时,ADP输出分别为+24.5V、0V,ADP5071温度降至29°,SW1和2波形如下:

    当Vin降至10V时,负输出已经没有了。。另外由于是固定DC12V适配器供电,通过降低输入电压方式改造不可行;*板子已做好没有预留输入电压调整功能

    另外想与您探讨2点问题:

    1、既然是使用条件逼近开关管压降限值,输入12V不变,通过降低输出的±26.5V也是一样效果对吧?

    2、如果按照Vin=12V,Vout=±26.5V,负载电流=200mA(←应该是最大带载能力)的话,ADP5071工作温度大致在多少度算正常?

  • 将输出电压更改为+26.5V、-24.5V,加大了负电压储能电感感值,更换了肖特基二极管,测试电感电流波形发生畸变具体如下图,请问这种电流波形代表什么含义?