Post Go back to editing

dc2987a基板测试咨询

Category: Hardware
Product Number: lt3935

我们在用dc2987a基板测试,j3 on状态使用滑动变阻器调节输出的电流。

断电时,调节VR1滑动电阻器,使用万用表测量CTRL 引脚对地电阻(VR1 引脚1、2),测量结果为0→34KΩ。根据电路图分析,不应该是0→100KΩ么,帮忙看一下原因

通电测试时,通过电路分析:CTRL 引脚对地电压=2V  X(VR1 引脚1、2阻值)/(R4 +VR1总阻值)可实测结果偏差较大,并且led实际电流与计算值有较大偏差,见图1。计算值根据图2.

请问这是什么情况?

此外,lt3935芯片4A回路原理图VR1和R2电阻接序,与dc2987a基板测试板接序不一样,见图5.以哪个为准?

 (图1)

 (图2)

测试场景

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.