Post Go back to editing

ADP5090 startup and charging issues

Category: Hardware
Product Number: ADP5090

I press the reference circuit for energy collection to build the circuit, and the capacitance on the BAT is 4.7 μ The aluminum electrolytic capacitor of F remains at around 0.372V when input into the rectifier bridge, while the voltage of BAT and SYS remains at around 0.578V and cannot be increased. However, I can use LTC3588 to store energy, making it 4.7 μ The capacitance of F rises to around 5V, and then discharges to light up the LED light. May I ask why this is? Please find attached my schematic and PCB layout.