Post Go back to editing

LT3092

Category: Hardware

想确认一下LT3092的典型电路推荐中显示DAC输出0-1V驱动电流0.5ma-100ma的电流,是否可用作0-100ma比例阀的驱动

Thread Notes

Parents
  • "I would like to check whether the typical circuit recommendation for the LT3092 shows that the DAC output 0 1V drive current 0 5ma 100ma can be used as a driver for a 0 100 ma proportional valve". 

    Yes, the LT3092 can be used to drive a proportional valve.  Try to always keep SET and OUT close to the same voltage.  If the circuit is unstable, add some resistance in series.  

Reply
  • "I would like to check whether the typical circuit recommendation for the LT3092 shows that the DAC output 0 1V drive current 0 5ma 100ma can be used as a driver for a 0 100 ma proportional valve". 

    Yes, the LT3092 can be used to drive a proportional valve.  Try to always keep SET and OUT close to the same voltage.  If the circuit is unstable, add some resistance in series.  

Children
No Data