Post Go back to editing

使用ADP7118WAUJZ-5.0这款电源芯片时,有时会发现它的输入引脚Vin会拉低外部电源输入电压,怎么回事

Thread Summary

用户在使用某电源芯片时遇到问题,当外部输入为DC16V时,Vout输出应为5V,但个别芯片输出为3V,且Vin也降为3V。建议进行AB BA测试,将问题芯片换到正常工作的PCB板上,以确定问题是否出在芯片本身。
AI Generated Content
Category: Hardware
Product Number: ADP7118WAUJZ-5.0-R7, ADP7118

 使用该款电源芯片时,外部输入为DC16V,Vout输出固定位5V,大部分PCB板上输出是OK的,但是在调试时发现个别电源芯片Vout是3V,显然是不对的,然后测量该电源芯片输入脚Vin也变成3V,把该电源芯片拆下来,量测PCB板其他电路都是OK的,所以猜测问题出在该电源芯片上。

接着把该芯片接入电路,VOUT输出翘起不焊接,处于空载,发现输入脚Vin还是显示3V,拆了几块旧板子上的焊上,仍然是该问题,请问大佬们知道这是什么问题吗?是芯片本身容易NG还是需要注意焊接工艺啥的?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.