Post Go back to editing

LT393驱动一个LD激光器频闪

使用LT3935时遇到以下问题:

1、驱动LD激光时Vout=2.4V,Vctrl=0.5V,但是激光器会频闪,此时Vout电平降低,在1.8-2.4V直接跳跃;

2、使用LTspice仿真发现Vout与实际一致,而且测量FB时,Vfb=0.65V;

3、调整Vctrl电源可以控制电流大小;

4、LD激光器功率最大为1.2W,工作参数2.2-2.6V/0.8A左右;

5、此芯片是否支持低功率的驱动,或者说支持的驱动功率最小是多少瓦;

6、手册中写道0V to 36V LED String Voltage,但是有一个图中电源仅仅大概在3V左右(LED Current vs VOUT)

Parents Reply Children
No Data