Post Go back to editing

关于在LT4363-2及LTC4364-2中的Retry Duty Cycle问题?

敬启者,您好:

在选择使用LT4363-2及LTC4364-2中有一个参数Retry Duty Cycle;

关于Retry Duty Cycle,我的理解是:

假定T1为Cctmr电容开始充电到MOS管关闭所需时间,Tcool为冷却时间;

Retry Duty Cycle=T1/(T1+Tcool) * 100%

LT4363-2:Less Than 1% Retry Duty Cycle During Faults, LT4363-2;

LTC4364-2:0.1% Retry Duty Cycle During Faults (LTC4364-2);

请问

1、关于Retry Duty Cycle的理解是否正确?

2、仅这个参数是否有优劣之分,在使用时如何选择?

Parents Reply Children
No Data