Does the output voltage of the LT3045-1 vary with the load resistance?
I want the input voltage to be 5.3V and the output voltage to be 5V and 500mA. I simulated the output voltage of LT3045-1 in LTspice and found that when Rset= 49.9K, the Vout does not have to be 5V and will change with the change of load.When the load is 10 Ω, the output is 5 V, 500 ma, when the load is 5 Ω, output is about 3.5 V, 700 ma, when output load is 15 Ω, output is 5.5 V, 300 ma.Isn't the output voltage related to Rset? Why does it change with the load resistance?Is there no stable voltage output?