ADP5070地线问题

ADI专家,你好,我现在有个应用,里面用了AD7194和运放AD8656,我用ADP5070+ADP7102,ADP7182做正负电源供电,其中+5v还作为AD7194的模拟电源,我想问的问题是AD5070中PGND和AGND应该怎么应用,我需要将ADP5070的AGND和AD7194的AGND相连接再和PGND单点连接吗?我现在的做法是将ADP5070的PGND、AGND与数字地都连接在一起,然后和AD7194的AGND单点连接,这样做会引入噪声吗?怎么做才合理呢?谢谢各位专家抽出宝贵时间帮我解决问题。@

attachments.zip
Parents
  • 我现在线性稳压器端输出的噪声就有50mV左右的峰峰值,这是不是由于我电源布线部分不合理造成的?

    ADP5070输入端噪声:

    ADP5070 +9V输出噪声:

    ADP7102 输出端噪声:

    ADP7182 输出端噪声:

    AD7194 模拟输入噪声:

    这些电源噪声是不是太大了?这几个点的噪声都在什么范围是正常的呢?现在我的AD采样达不到精度要求,只有9位的稳定值,是不是电源噪声引起的?将电源部分的PGND和AGND分开铺设是否能有效降低噪声?是不是需要采用4层PCB?

Reply
  • 我现在线性稳压器端输出的噪声就有50mV左右的峰峰值,这是不是由于我电源布线部分不合理造成的?

    ADP5070输入端噪声:

    ADP5070 +9V输出噪声:

    ADP7102 输出端噪声:

    ADP7182 输出端噪声:

    AD7194 模拟输入噪声:

    这些电源噪声是不是太大了?这几个点的噪声都在什么范围是正常的呢?现在我的AD采样达不到精度要求,只有9位的稳定值,是不是电源噪声引起的?将电源部分的PGND和AGND分开铺设是否能有效降低噪声?是不是需要采用4层PCB?

Children
No Data