准备设计一款输入48V,输出12V/20A有源钳位正激电源,在使用ADP1051时,遇到了一些问题,烦请帮忙解答。
1.ADP1051与PC机无法连接。ADP1051外围电路参考数据手册及应用手册进行设计,PC机安装了官方提供的GUI,在采用USB-to-i2c适配器(采用手边的TI公司的USB-to-i2c Adaptor)连接PC机和ADP1051后,GUI无法识别芯片。想请问,该问题是否出在适配器不匹配,或者还有别的什么原因,如果是适配器的问题,是不是需要专用的适配器,在哪里可以购买。
2.在GUI中,设置PWM波形与基本拓扑有关吗,死区时间怎么根据所用拓扑结构进行设置,GUI中的一些设置有些看不懂,数据手册对这部分介绍不够详细,是否可以更详细一点的关于GUI使用的资料吗,或者在哪里能找到有源钳位正激的.51S文件,我可以参考学习,如果能有专业的技术支持联系我就更好了,谢谢!
我的邮箱地址是lizhuang771@163.com。