LTC2325-12
1 应用:通过MCU软件控制ADC进行不定时的单次采样,可能数秒钟1次或者连续以200ns时间间隔采集n组数据等突发式的采集。ADC不进入待机状态。这种数秒钟1次的单次或者突发多次采集相对于固定周期采集(比如固定1MSPS)会有损失吗?可以如此应用吗?
2 数据手册10页上的 Step Response(OUTPUT CODE vs SETTLING TIME)图不太明白:输入是5MHz方波,采样率也是5M,横轴SETTLING TIME是指的啥?输入5MHz方波与adc的CNV之间的时间差吗?是不是说,如果采集脉冲信号,比如100ns宽度(对应图上的5MHz方波)的矩形脉冲,只要cnv时间差大于40ns左右,就可以获得脉冲信号正确的幅度?
3 组合以上1和2,如果矩形脉冲较宽,比如200ns~1us,但是其出现频率较低,比如,数分钟一次或者数us一次,那么,使用该adc,是不是适用?比如控制时间差可以单次采集到200ns矩形脉冲的幅值,也可以在1us宽矩形脉冲幅值处采集多个组数据?
谢谢! :)
题外:跟之前的问题类似,同样问一下该器件是否可行,准备替换AD7356,因为这个可以同时采样4路,而AD7356只能同时才2路。