Post Go back to editing

关于LT8300输入电压范围与输出的问题

LT8300的输入电压范围是36~72V,但使用LTspice对LT8300进行仿真,发现在输入电压为36V时,可以正常输出5V,12V,15V的电压值,但是当输入电压变为48V,72V时,无法获得正常的12V、15V电压,输出电压低于想要的输出值,电路中的各种参数均按要求设置,不知道是什么原因。这与LT8300的输入电压范围是36~72V是不是矛盾了?

attachments.zip