求助帖 LTC3119 太阳能给锂电池充电电路设计问题?

我计划用LTC3119做一个太阳能(电压可能高于锂电池也可能低于锂电池电压)给锂电池(两节,7.4V标称,充满8.2~8.4V)充电的电路,左边的蓝框框用一个数字电位器(DP)来通过MCU调节太阳能的最大功率点。打算将右边的红框框里的分压电阻去掉,让器件的PVout引脚直接挂在锂电池上,是否可行?

我读了一下datasheet,里面提到“At any given time, only one control loop is active while the other is inactive. Priority is given to the MPPC control loop, which can override the voltage loop and reduce the commanded current level. When under control of the MPPC error amplifier, the compensation network of the VC pin is ignored.”也就是说,当MPPC起作用时(调节太阳能最大输入功率),FB不起作用,是否意味着FB不会调节PVout的电压,也就是说可以不用连接分压电阻了?

锂电池在充电过程中,电压在6~8.4V之间上升,PVout的电压由锂电池电压决定,当锂电池快充满时,假设这个时候锂电池电压(也就是PVout)可测,能否通过MCU继续调节左边的数字电位器,使PVout维持8.4V恒定(这时不需要太阳能工作再最大功率点了)?

第一次设计这样的电路,没经验,麻烦各位赐教,谢谢

Parents Reply Children
No Data