原理图如上图所示,VM连接唯一的负载是H桥,当VBATOUT物理断开时,由于H桥关断,因此滤波电容上的VM只能从反馈电阻R16和R21续流,由于R16和R21非常大,因此VM电压下降非常慢,需要好几分钟。而且因为VIN物理断开了,且该芯片内部MOS没有寄生二极管,因此不能从电源端放电。
C19和C26是根据仿真软件补偿做的,中途把这两个电容拆掉过,也任然是上述情况。
上述分析如有问题,请指正。
不知有何好办法能让VM快速降至0V。
我想了几个办法
1.减小反馈电阻。
2.加一个固定的阻性负载。
但以上两种方法都会增加功耗。不知有无更好的方法可以解决?
There must be a current path to discharge the load. I don't have a better solution other than yours.