使用LT3083EQ问题。

使用LT3083EQ问题,使用DAC输出控制SET来调节输出电压,输出电流需求3.5A,因此两片SET并联。

       问题1:输入and使能均为12V,输出0~10V可调,实际输出压降2.26V左右,而不是0.5V。

       问题2:输出5V时,如果调节输入6.5V~12.5V,过程中会有鸣叫现象。

      问题3: 两片并联实测输出2A,发热严重。

盼回复,谢谢。

Parents Reply Children
No Data