LTC3829?

用LTC3829做一个项目,输入电压19~32V,典型28V,输出设计1V/80A,设计的时候有几个疑问:1,这种外置MOS的电源芯片一般数据手册都没有太明确标注电流的输出能力,只是查的时候才看到有输出90A的能力,那么这种芯片的电流输出能力一般怎么决定的,我现在这个设计,输出1V/80A从理论上是否可行呢?2,用ADI的LTPOWER仿真的时候,这两个地方怎么解决一下呢,或者重新配置一下参数?(图中红色框框) 3,外面那个电流感应,用的1m欧的电阻,感觉损耗有点大了,会降低效率,如果用电感反馈,和用电阻有什么不同?多谢您的解答

  • 0
    •  Analog Employees 
    on Aug 9, 2019 12:35 AM

    1.控制器的方案输出电流可以大,因为发热器件在外面,但同时也要考虑芯片驱动外部MOS管的能力,如果输出电流越大,你需要的MOS也就越大,那么需要控制器驱动这些MOS,会给控制器带来发热。2.你需要更小的Rsense电阻,另外从28V转1V占空比很小,ton时间太小满足不了规格,你可以用更低的开关频率去试一下。