LTC4040备份模式下提供电流大小

在产品中准备使用LTC4040 3.7V锂离子电池作为后备电源,试验过程中,发现充电过程正常,但在备份模式下(输出电压调整电阻调整为5V,电池电压3.7V时),只能提供800mA的电流,可能的原因是什么?(试验时,用的5Ω电阻作为负载,显示负载两端电压为4.1V)

Parents
  • 0
    •  Analog Employees 
    on Aug 1, 2019 3:18 PM over 1 year ago

    你好,

    你应该检查你的输出电压设置,以确保你真正提升到5V。检查BSTFB引脚电压。如果使用较小的负载,它是否达到5V?如果是这样,你就会在某个地方限制权力。检查元件值(电感)并确保在发生这种情况时电池没有下垂太多。

    问候,

    扎克

  • 输出电压设置电阻满足datasheet的要求,BSTFB的两只电阻分别是680KΩ和130KΩ。

    图1万用表是电池电压,右侧是电子负载,采用恒阻模式,负载是20Ω时,输出电压4.92V,此时电流约为250mA。


    图2是负载5Ω时,输出电压为4.05V,电池电压3.599V。

    图3是负载5Ω时,SW引脚(pin21/22)的波形图,可以看到并没有达到1.25MHz的开关频率

    图4是空载时,SW引脚的波形,可以看到算是可以达到1.25MHz,但也是时断时续。

    图5是原理图。

Reply
  • 输出电压设置电阻满足datasheet的要求,BSTFB的两只电阻分别是680KΩ和130KΩ。

    图1万用表是电池电压,右侧是电子负载,采用恒阻模式,负载是20Ω时,输出电压4.92V,此时电流约为250mA。


    图2是负载5Ω时,输出电压为4.05V,电池电压3.599V。

    图3是负载5Ω时,SW引脚(pin21/22)的波形图,可以看到并没有达到1.25MHz的开关频率

    图4是空载时,SW引脚的波形,可以看到算是可以达到1.25MHz,但也是时断时续。

    图5是原理图。

Children