求推荐一款升压器,一串2.3V/20h钛酸锂电池输入 输入电压范围1.5V--2.7,升压到5V 想输出5A电流 有可能实现吗?单片不行 可以并联使用吗??求推荐,谢谢
问答
讨论
文档
Members
Tags
Cancel
Thread Details
State
Verified Answer
+1
person also asked this
people also asked this
Replies
2 replies
Subscribers
15 subscribers
Views
1473 views
Users
0 members are here
Options
Share
More
Cancel
Related
Post
Go back to editing
求推荐一款升压器,一串2.3V/20h钛酸锂电池输入 输入电压范围1.5V--2.7,升压到5V 想输出5A电流 有可能实现吗?单片不行 可以并联使用吗??求推荐,谢谢
limitmoon
on Mar 8, 2019
如题。。
ADIApproved
on Mar 26, 2019 4:54 AM
+1
LTC3124
Cancel
Up
+1
Down
Reply
Reject Answer
Cancel
FormerMember
on May 8, 2019 1:22 AM
in reply to
ADIApproved
0
谢谢 我看看
Cancel
Up
0
Down
Reply
Verify Answer
Cancel