三个LTM4678电源模块并联使用,上电初始电压1.0v,上电完成之后要求通过PMBUS改成0.85v,在修改过程中,3个模块之间电压不一样,会不会出问题?

需求:12v输入,初始电压1.0v,上电之后通过PMBUS改为0.85v,电流150A;

当前设计:

1、三个LTM4678电源模块并联实现,上电初始电压1.0v,上电完成之后要求通过PMBUS接口改成0.85v,但是在修改过程中,3个模块电压不可能同时修改成0.85v,肯定有先后顺序。如果第一个模块电压改为0.85v,但是余下两个模块的电压还没有改过来,这个是否有影响?是否有参考设计?

2、如果第一种方案不行,是否可以用1个ltm4678+2个LTM4650,这样是否可以使用?有没有参考设计?

Parents Reply Children
No Data