Post Go back to editing

推挽谐振的工作原理,LT1534的参考设计 from << Application Note 118 >>

阅读了LT的Application Note 118--High Voltage, Low Noise, DC/DC Converters,

对于里面基于LT1534的两个参考电路(Page4,Page5)的推挽谐振工作波形和工作阶段一直都没研究明白,特提出该问题,希望能得到解答。

1. 因为这款芯片应该比较老了(对应的这个AN118是2008年的版本,内容介绍得很多),并不能找到对应LT1534的PSpice模型或LTSpice模型,所以首先想请问是否有相应的新的替代产品?

需要设计的是一款输入电压约12V-15VDC,输出高电压(最高达1250VDC)、低纹波(0.5mV)的APD、PMT驱动,要求电压可调(包括正、负电压),低电流(最大2.5mA)。

2.因为没有找到对应LT1534的PSpice模型,所以自己摸索着建立了如下图所示的PSpice仿真电路,只仿真了初级电路,用了一个电压控制开关代替LT1534,仿真后的图形如图所示,能够得到振荡图形,但是发现调试开关占空比或者开关频率,都无法改变初级中心抽头线圈两端的AC电压(个人认为即无法改变输出电压)。

想请教,有没有大神能详细解释一下这个电路的工作过程(从上电至电路开始振荡),尤其是初级中心抽头电感和两个0.22uF的电容组成的谐振电路是怎么工作的,这个地方特别搞不明白。