ADI微博网友@Icey_P问:我需要一个服电源输出的芯片,请问有什么推荐呢? 要求,输入电压9V,输出电压-7.5V(最好可调,并且调节方便),输出电流,大于100mA,小于1.5A,纹波最好较小,但是没有严格要求。封装不要是BGA的,因为没办法测试。TI的PTN78000A模块稍贵
ADI专家回答:输入9V,输出-7.5V,并且电流可以到1.5A的解决方案您可以选择:ADP2384(做成buck-boost结构)或者ADP1621(这是一款控制器)+mosfet。输出电压的调整您可以通过调整反馈电阻比例来实现。