Post Go back to editing

LT4363应用问题

我用LT4363设计了最简单的保护电路,输入电压65V,但是输出电压无法达到65V,最高的时候只能调节到30多V,不知道什么原因?我的电路描述如下:

1. Vcc管脚直接连接到Vin,也就是输入65V;

2. OV短路到GND;

3. UV直接连接到Vin;

4. /SHDN开路;

5. FB连接到GND;

6. TMR接0.047uF;

7. MOS管是FDP3632,栅极与LT4363的GATE之间10欧姆电阻;

8. 负载为开路。

按照这些参数时,输出电压约2.5V,如果FB端连接5k到GND,输出电压约30多V。不知道为什么会有这个现象?从Datasheet说明来看,如果不是用输出电压钳位功能,那么FB是直接接地。为什么我的电路这个情况下输出只有2.5V左右?

如果FB端接5k到GND时,FB的电压有30多V,这个正常吗?

希望能帮忙分析下此问题,谢谢。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.