Article 为什么MAX17222的EN引脚接到IN,其电压却等于OUT?

MAX17222的EN引脚在内部通过电阻连接连接到IN和OUT。IN与EN引脚在外部通常使用33MΩ的电阻连接,所以上电时EN的电压等于IN的电压。MAX17222使能工作后,当OUT输出电压就绪,MAX17222会在内部将EN切换到OUT,从而保持使能状态。这样做的目的是:当IN的电压较低时确保MAX17222正常工作。如果IN是电池供电的,可以充分利用电池的能量。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.