MAX86141AENP+: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX8x
MAX86141AENP+: FAQ
Created
over 6 years ago
Was this helpful?
Yes
No
More
Cancel
MAX30110和MAX30102适用应用区别
MAX30102是集成LED和光传感器的血氧及心率传感器。而MAX30110是血氧及心率传感器的模拟前端,需要外接LED和光传感器。二者各有优势。MAX30102集成方案多适应于手指测量,而MAX30110分立方案多适用于手腕的测量。
MAX86141与传感器PD的连线很长(20cm),对波形是否有影响?
当然有影响,PD出来是弱的模拟信号,不建议使用较长的引线,容易耦合噪声。可以把MAX86141和PD、LED放在一起,再通过FCC连接到控制器。
MAX86141数据手册里面写到可以测量StO2和SmO2,是怎样实现的
氧饱和度指的是氧合血红蛋白占全部可结合血红蛋白的百分比,其数值在0%到100%之间变化,其缩写为S(X)O2,其中: 因此,要测量StO2和SmO2,只需要选取不同的测量位置即可,比如将传感器放在腿部肌肉群上获取SmO2,放在嘴唇上获取StO2。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.