MAX77813EWP+: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX7x
MAX77813EWP+: FAQ
Created
over 6 years ago
Was this helpful?
Yes
No
More
Cancel
为什么MAX77813输出电压比设置电压高
MAX77813是可以通过I2C总线设置的buck-boost变换器,客户反映有时其输出电压与设置值不符合,会比设置值高一些,比如设置0x68对应输出电压4.68V,实际测得4.75V左右。造成这一问题的原因是之一是,客户实际工作电流较小。由于负载变化时,MAX77813会自动在PWM模式和skip模式之间切换以优化效率,MAX77813切换到了skip模式,此时的实际输出电压并非精确等于设置值,而是在设置值的101…
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.