MAX706ASESA+: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX7x
MAX706ASESA+: FAQ
Created
over 7 years ago
Was this helpful?
Yes
No
More
Cancel
MAX706AR_和MAX706R_性能上有什么区别?
MAX706R内部的看门狗功能不能被禁止,MAX706AR的看门狗功能在WDI处于开路或者连接到高阻输出时被禁止。
MAX706S的最低工作电压为1V,此时如何保证RFI 1.25V基准电压?
MAX706S能够保证在VCC低至1V时,保持有效的低电平复位状态。但不能保证1.25V的PFI比较器参考电压。对于复位电路中的独立比较器,通常用于电源电压失效前的预警,即在VCC跌落到复位门限之前产生报警。当VCC电压低至1V时,PFI比较器的监测任务已经完成,其输出不影响系统状态;另外,如果将PFI比较器用于监测另一路电源,则须注意PFI输入电压不应高于VCC+0.3V (1.3V@ VCC …
在WDI信号没有的时候,MAX706看门狗输出WDO输出的低电平脉宽持续时间是多少?
MAX706R的复位输出与看门狗监测是相互独立的,即看门狗复位不会触发/RESET复位。这样的话,如果客户没有将WDO输出连接到/MR输入,发生看门狗超时(/WDO输出低电平)后,如果没有手动复位和电压跌落触发/RESET的话,能够将/WDO恢复到高电平的只有WDI输入信号,所以,/WDO处于低电平的时间与何时收到WDI信号有关。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.