MAX701CPA+: FAQ

  • Created
Was this helpful?
  • MAX1701能否在1V输入电压下启动/工作?

    MAX1701的最小启动电压为1.1V(最大值),负载电流为1mA。负载电流为100mA时,器件的启动电压为大约1.8V。 请参考IC数据手册第6页START-UP INPUT VOLTAGE vs. OUTPUT CURRENT。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.