MAX6696: FAQ
文档
Forums
Members
Tags
Cancel
文档
MAX6x
MAX6696: FAQ
Created
over 7 years ago
Updated
2 months ago
Was this helpful?
Yes
No
More
Cancel
MAX6696读取温度异常
Question Description: ----------------------------------------------------------------------------------------------------------------------- 我们应用中不采用remote1、local、remote1、remote2自动轮询的方式,而是采用软件配置寄存器切换读取通道的方式…
请问下通过写09H寄存器切换两个external ch1/2后,需要等待多久才能正常读数?
内部的温度转换时间是受转换速率寄存器(0Ah)控制的,三路温度轮流转换,转换顺序是remote1, local, remote1, remote2。所以remote 1的转换速率比remote2 快2倍, remote1 大概125ms转换一次,remote2则是250ms 转换一次。
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.