MAX668EUB+T: FAQ

  • Created
Was this helpful?
  • 为什么MAX668使能关断后输出电压仍然存在?

    MAX668使能关断后其内部LDO的输出为0V,EXT引脚的驱动输出也为0V,但是由于MAX668没有真关断功能,即使关断芯片工作,由于输入与输出之间通过电感和肖特基二极管提供了一条直流通路,输出电压会比输入电压低0.2V左右,输出不为0V。
  • 如何将MAX668EVKIT的输出更改为5V@4A

    MAX668原来的输出电压是12V@1A, 如果想得到5V@4A可以更改以下参数: a. 输入电容 C1: 150uF 20%, 6.3V, X5R ceramic capacitor (1206) Murata GRM31CR60J157ME11# b. 电感 Coilcraft SER1052-152ML-152L c. 用于设置频率的电阻 R4: 110k ohm d. 检流电阻 R1: 使用3个…
  • 用 MAX668设计一个输出为12V/1.5A的电路

    MAX668EVKIT的输出为12V/1A,只需在评估板上做如下改动即可得到12V/1.5A a. 将电感更换为一个饱和电流在7.4A以上,3.3uH的电感,比如Coilcraft XAL5030-332MEC b. 将检流电阻R1更换为0.010Ω, 1%, 1/2W 的电阻 c.将整流二极管D1: 更换为一个额定电流为4A,反向压降在40V以上的肖特基二极管,比如 Vishay SSB44

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.